• TI Thinks Resolved

DLP3010EVM-LC: The projector doesn't work and the splash image doesn't show.

Prodigy 110 points

Replies: 9

Views: 163

Part Number: DLP3010EVM-LC

When I connected  the DLP3010EVM to the computer by the usb-cable,the projector did not work and the splash image did not show.I found that the D8,D9 and D11 leds blinked together four times.

Before the problem occurs, I was testing the  Light Control(Internal Patterns) . I clicked the Program and Load Pattern Data, then the progress bar was stuck. Wait about 1 minute, I cut off the power. When I power again, the projector didn't work.