This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350: DLPC350 buffer freeze

Prodigy 40 points

Replies: 5

Views: 192

Part Number: DLPC350

Hi,

I make a new design on the DLPC350 + DLP4500 and the Port 2 (FPD-LINK interface ) has been selected as the video port.

The DMD projection function is ok when i use the internal pattern to test it.

In video mode, the DMD can continue to project hundreds of image stream from FPD-LINK interface .

But i found DLPC350 frame buffer frozen after it receved hundreds of frames. I monitor current read buffer pointer but the value of feed back is not exchange.

I can't find any description about what will lead to the buffer freeze in datasheet or UG.

I have checked the frame timing, it match the spec.

what can I do to troubleshoot the issue?

5 Replies

  • Expert 5355 points

    Hi jning,

    What firmware are you currently using?

    Regards

    azad

  • In reply to Azad:

    Hi,

    DLPR350PROM_v3.1.0.bin which is from TI.

  • In reply to Azad:

    Hi,

    It can get the firmware version from DLP LightCrafter 4500 Control Software.

  • In reply to jning Li:

    Hi Jhing Li, 

    As understood from the description above, you are operating the device in "Pattern sequence from video source" mode, am I correct? In that case, can you provide us the INI of the pattern configuration you are using? Also kindly provide the video timings you are using. This will help us to reproduce the issue at our end. 

    Thanks & Regards,

    Hirak.
     

  • In reply to Hirak Biswas:

    Hi Jhing Li, 

    Do you still need the answer to your question? We'll be temporarily closing this thread due to inactivity, you can reopen anytime!

    Thanks & Regards,

    Hirak.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.