This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPNIRNANOEVM: DLP Nanoscan controlled by ESP32 - What data to send?

Prodigy 120 points

Replies: 3

Views: 117

Part Number: DLPNIRNANOEVM

Hi,

I'm communicating with the NIRscan nano evm over UART by sending and receiving commands.

I'm able to send commands to put the lamp on and off, get the device status, ...

So I'm able to send en receive commands.

The next thing to do is to receive the files which are stored on the SD card. 

But I'm struggling with sending the proper 'data' in the command. 

First, I wan't to perform the 'Read file list size' command over UART. 

The user guide says that it needs 1 byte for the Data Payload Input, but it is unclear for me what it should be. 

It just says 'NNO_FILE_SCAN_LIST'

Can you help me with this?

Regards

Nick 

3 Replies

  • Hello Nick,


    Please give us a few days to look into this as our expert on this platform is out until next week.


    Thanks,
    Kyle 

  • In reply to Kyle Rakos:

    Hi Nick, 

    We'll look into this and get back to you next week. Thanks for your patience. 

    Thanks & Regards,

    Hirak.

  • In reply to Hirak Biswas:

    Hi Nick, 

    Closing thread as it is a duplicate.


    Thanks & Regards,

    Hirak.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.