This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DLPDLCR2000EVM: BBB Cape Overlay Customization

Part Number: DLPDLCR2000EVM

All,

When using the DLP LightCrafter Display 2000 EVM, there are some situations where you may want to use the EVM with a system that does not have native support for the EVM's drivers. An example of this is using a custom operating system image based on an older release of Debian that has various software packages or drivers that is useful for a particular project. Below is a download for the cape overlay file and EEPROM data which can be used to install the driver on any BeagleBone release from scratch.

/cfs-file/__key/communityserver-discussions-components-files/94/7077.DLPDLCR2000_2D00_00A0.dts

/cfs-file/__key/communityserver-discussions-components-files/94/3583.dpp2601_5F00_eeprom.dump

To install the cape overlay, follow the instructions available at the following page:

https://github.com/beagleboard/bb.org-overlays

https://cdn-learn.adafruit.com/downloads/pdf/introduction-to-the-beaglebone-black-device-tree.pdf