This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DLPDLCR2000EVM: Using TFP401 HDMI/DVI Decoder as input to DLPDLCR2000EVM

Prodigy 120 points

Replies: 1

Views: 635

Part Number: DLPDLCR2000EVM

Hi,

Can I use TFP401 HDMI/DVI Decoder as input to DLPDLCR2000EVM?

HDMI In ---> TFP401 HDMI/DVI Decoder --->Parallel Video Data ---> DLPDLCR2000EVM --> Projector

  • Jayakrishnan,

    The TFP401 outputs RGB888 parallel video, which is the video format compatible with the DLPC2607 (and DLPDLCR2000EVM). As such, a custom design using this part will indeed provide HDMI input capability to the EVM.

    I hope this helps.

    Best Regards,
    Philippe Dollo

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.