This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] DLPLCR6500EVM: Pattern mode configuration for the DLP LightCrafter 6500 vs. DLP LightCrafter 4500

Prodigy 675 points

Replies: 1

Views: 816

Part Number: DLPLCR6500EVM

Pattern mode configuration for the DLP LightCrafter 6500 doesn't allow me to specify the bit position for my pattern like the DLP LightCrafter 4500. Why not?

  • In the DLP LightCrafter 6500 GUI, this feature was removed to help simplify the user experience. The controller automatically takes care of addressing the bit planes of the image and the index number for each image. The GUI also allows users to use batch files which are highly flexible and easy to use.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.