This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] DLPC200: Using SPI with DLPC200 and DLPC5500

Prodigy 675 points

Replies: 1

Views: 1230

Part Number: DLPC200

How do I configure the DLPC200 controller using SPI?

  • The DLPC200 has a slave SPI port. Information on commands to use and utilizing this interface can be found here, The SPI commands can be sent via external processor or microcontroller.

    Also take a look at this E2E thread which works through a number of customer issues using SPI:

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.