Other Parts Discussed in Thread: TIDA-00254
Hello,
I am using the DLP4500 for 3D Pointcloud generation. My setup also includes a BFLY-PGE-13E4C/M-CS Point Grey BlackFly camera (Global Shutter). I have made the connections according to the manual. The connections between the camera and the DLP4500 are as follows:
DLP4500 - J11 || PointGrey BlackFly Camera (6-pin GPIO connector)
Pin 2 --> Pin 3 (Red Wire)
Pin 3 --> Pin 5 (Blue Wire)
The GPIO connecter labelling for the camera mentined above was referenced from here : https://www.ptgrey.com/support/downloads/10202
I have followed all the steps for installing and running the DLP_LightCrafter_4500_3D_Scan_Application. On startup however I get the ERROR: PG_FLYCAP_C_SET_FORMAT_7_FAILED message. The full output on startup is as follows:
Connecting to projector...
Configuring projector...
Connecting to camera...
Configuring camera...
Camera setup FAILED!
ERRORS: 2 and WARNINGS: 0
ERROR: PG_FLYCAP_C_SET_FORMAT_7_FAILED
ERROR: CAMERA_NOT_SETUP
Step 2: Prepare DLP LightCrafter 4500 (once per projector) also runs perfectly but in the camera calibration step (Step 4) I get the following errors:
Loading camera calibration settings...
Setting up camera calibration
Camera calibration setup FAILED:
ERRORS: 4 and WARNINGS: 0
ERROR: CALIBRATION_PARAMETERS_MODEL_SIZE_MISSING
ERROR: CALIBRATION_PARAMETERS_MODEL_SIZE_MISSING
ERROR: CALIBRATION_PARAMETERS_IMAGE_SIZE_MISSING
ERROR: CALIBRATION_PARAMETERS_IMAGE_SIZE_MISSING
I have checked my camera in the FlyCap software and I'm able to get live video and capture images from it perfectly. I would appreciate any help on this problem. Thank you.