Hi all,
As a test I would like to displaysix images on the 4500EVM and capture them manually through my camera. See images below
I have looked at the training videos and I just want to clarify that I am doing this correct or if there may be an easier alternative.
Each image is 8 bit
As best I can tell I should
- Create a 24 bit image with the first three images.
- Create a 24 bit image with the second three images.
- Create a version of the firmware with these two new 24 bit images
- Upload the firmware
Questions
- The DLP Lightcrafter GUI is different than the training videos. How do I create my own .bin file with my new patterns
- When they are uploaded to the lightcrafter what is the simplest way to display each of the 6 images manually? Basically I just want to take a picture on the object with each of the patterns
- Is the approach I am taking correct? Is there an easier way? (not normal video mode as the video card is altering these images before sending them to the lightcrafter - gamma etc..)
- Can I use windows 10 to upload the new firmware?
Thanks