This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010EVM-LC: MIPI DSI on LPD 2010

Part Number: DLP2010EVM-LC

Hello,

I need to prototype a MIPI-DSI interface into the DLP2010 EVM.

My plan is to create a new daughter board with the DLPC3430 and the MIPI-DSI interface broken out to a separate connector.

My questions are:

  1. Will the firmware stored in the optical engine Flash memory still work with the DLPC3430? If we need to replace the Flash contents, are all the tools needed available?
  2. Can the DLP GUI work with this setup?
  3. Assuming that the MIPI-DSI bus is attached through a separate connector, will we need to modify the main board?

Best regards,

Rasmus