Hello,
I have an issue with my card DLP6500, either there is a special usage method, or it is me who broke it. the problem is that it happened two times "breaking the card/ DMD". so I'm wondering if there is a special way to use it ?
The problem is that I bought a DMD DLP6500 (sscreen + controller) and It was working very well, but whenever I wanted to reboot it, I plug and unplug the cable withou doing any standby. and when I did it the second time. I unplugged the alimentation cable, after a while when I wanted to upload images, the firmware was corrupted and I need to use the JTAG .... so please can you tell me if the way of using is bad and if there a special way to ON/OFF the card. (by keeping it standby mode) thanks
Omar