Part Number: DLPLIGHTCRAFTER
I'm looking to get DLP light crafter 6500 or 9000 but operating between wavelenths 1200 nm and 1700 nm. Where to get such a panel?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLPLIGHTCRAFTER
I'm looking to get DLP light crafter 6500 or 9000 but operating between wavelenths 1200 nm and 1700 nm. Where to get such a panel?
Hello Nicholas,
We do not offer an NIR DMD for the DLPLCR6500EVM or DLPLCR9000EVM. It is possible to run them outside of this specification, but there would be no warranty. The window is definitely NOT optimized for the wavelength range you are talking about.
There is a new DMD offering that has a window optimized for the NIR. This is the DLP650LNIR [WXGA]. (Note this is a different resolution than the DLP6500 - [1080] ). This DMD has a window optimized for the NIR from 850 nm to 2000 nm. The window characteristics can be found in this document --> Wavelength Transmittance Considerations for DLP® DMD Window [click on link]
The DMD with DMD board and flex is available now [ DLP650LNIR DMD evaluation module ], but the Controller EVM to run it has not yet been released but we expect it in the next month or two.
Fizix