Tool/software: Linux
Hello. I uset the Debian 8.9, and updated as the instructions told. But im missing the DLPDLCR2000 driver file. The device/bone/capes folders are missing too
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
Hello. I uset the Debian 8.9, and updated as the instructions told. But im missing the DLPDLCR2000 driver file. The device/bone/capes folders are missing too
i reinstalled the image on another sd card and now the drivers apear in the folder as it should. and i installed it without any problems,
i use beaglebone black wireles,
when i plug light cracter direct ti 5 v power it lights up
when i put it on the bbb it wont start unles i write the 4 lines
>sudo su
echo 48> /sys/class/gpio/direction and so on, pin 15/gpio_48 needs to bi high as i understand. and then it lights up fine with the test screen, until restart, then i need to type the codes in the terminal again to light up test screen, how can i avoid that
when i try the aquarium test, it looks fine on the 10"inch monitor but the image is wery blurry on the projector and i can see the mouse cursor dublicated in some kind of pattern
i realy hope you can help me i have been fighting with this for over a week