Hi all,
I have a DLPDLCR3010EVM-G2 projector that creates a large image, even if the distance to the screen is short.
I could remove and replace the built-in "lense pack" to make the size of the projected image smaller, but I'd prefer to keep the device unchanged.
1. What type(s) of lense(s) in front of the unchanged device would be required to make the image dramatically smaller?
2. Can positive (converging) lens achieve this trick?
The expected projection area could be 5cm×5cm or even smaller. The quality of the image and the resolution should still be good afterwards.
Thanks for your time!