Hello!
I am using a DLP4500 with its Evaluation Module. I am trying to send some patterns via HDMI in pattern mode.
If I understood correrctly, in this case the trigger is given by the Vsync coming from the RGB video source (I am using a laptop to control the DMD so it is 60Hz). What I would need is to send a pattern and to make sure the mirrors stay fixed in the "pattern position" for long time (0.1-1 sec), until another pattern is sent from the source.
So the questions are:
1) does the DMD stay in the "pattern position" if this one is the same over many "trigger periods" (let's say if my pattern is the same for 300ms), or it changes to another position and goes back everytime it receives an input from the Vsync?
2) in this second case is there a easy way to change the settings to make sure the mirrors are fixed if the pattern does not change (for example changing the exposure time of the patterns), or I am forced to change the Vsync somehow?
I hope my questions are clear (I am not very experienced with this).
(I already asked a question related to this some days ago but I think I didn't fully understand my issue back then and I thought it was resolved, so I apologize for this multiple thread).
Thnk you very much!
Regards,
Luca Zanotto