Hello,
I have a design which uses the DLPC3430 and it receives pixel data over the DSI interface. Under normal operation (both host DSI processor and DLP are operating) the output is fine.
The issue occurs when the host processor DSI interface is disabled and then re-enabled. In most instances, the DLP DSI interface is not affected and the output is updated correctly. But occasionally the DLP DSI interface seems to lock up and not update the output. When this occurs, the video output can be changed to test mode and test mode images can be output correctly, so the device is not completely locked up.
In order to get the DSI interface working again the DLP3430 needs to have the PROG_ON signal cycled to re-initialize the device.
Are there any I2C commands that can be used to 1) reset the DSI port and 2) monitor the status of the DSI port?
Thanks,
Chuck