Tool/software: Linux
Dear DLP team,
The issue I am having is that after setting up the connection with the beaglebone and sending the initial command no DLP LightCrafter Display splash screen is projected. All I see is a flashing red screen.
I followed the user guide/ tutorial and also installed the newest debian version but couldn't get it to work. I attached the code I used to set up the DLP below.
Is there a way to check if the DLP is working properly? Thanks for your help.
#Turning the EVM ON #Connect BeagleBoard to computer with mini USB cable- wait ~2 min $ ssh debian@192.168.6.2 #Password is temppwd #Connect power supply to Lightcrafter $ sudo su $ echo 48 > /sys/class/gpio/export $ echo out > /sys/class/gpio/gpio48/direction $ echo 1 > /sys/class/gpio/gpio48/value # activating i2c ports $ i2cset -y 2 0x1b 0x0b 0x00 0x00 0x00 0x00 i $ i2cset -y 2 0x1b 0x0c 0x00 0x00 0x00 0x1b i