Part Number: DLPLCR6500EVM
Today when I started to use the DLPLCR6500EVM as usual, I cannot connect it to my computer via USB. And I can hear a beep sound from it after power is on.
what should I do to make it work?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLPLCR6500EVM
Today when I started to use the DLPLCR6500EVM as usual, I cannot connect it to my computer via USB. And I can hear a beep sound from it after power is on.
what should I do to make it work?
Hi,
Thx for your kind reply.
Update the problem description: The device can now connect to the computer, but the EVM is stuck on the standby mode even though I change it to normal mode. Similarly, it remains in video mode and I cannot change to any other mode such as on-the-fly mode. Once I click the 'on-the-fly' button, the button returns to video mode in the 2-3 sec and without any prompts.
I found other people reported the same question with me in https://e2e.ti.com/support/dlp/f/94/t/789002
I would be very glad if I can get any suggestions or solutions to this problem. Thanks!
Yang Dong
Hi Dongsheng,
Please post the screenshot of GUI front page when usb is connected.
Also try reprogramming the EVM using boothold jumper J11 in case firmware has corrupted.
-ykc