Other Parts Discussed in Thread: DLPC3478, DLP4500, DLPDLC-GUI
Hi,
We use DLP3010EVM-LC.
Does it need JTAG for first program to Flash memory ?
Is it available to use only USB for for first program ?
Best Regards
Hiroyasu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We use DLP3010EVM-LC.
Does it need JTAG for first program to Flash memory ?
Is it available to use only USB for for first program ?
Best Regards
Hiroyasu
Hiroyasu,
The GUI can be used to program the flash after first assembly if the following conditions are met:
1. Projector switch is in OFF position
2. The MSP430 has been programmed
3. Cypress bridge is correctly configured.
If the above conditions are not met, JTAG must be used to to program flash, please access the SPI flash IC directly using an adapter like Cheetah.
JTAG cannot be used to program flash.
Regards
Azad