This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2010EVM: 240 Hz Firmware Support

Genius 16300 points

Replies: 1

Views: 1357

Part Number: DLPDLCR2010EVM

To all DLP® Products users,

Our team would like to make an announcement regarding an exciting update for the DLP® LightCrafter™ Display 2010 Evaluation Module. We have released an update available on TI.com which adds support for 240 Hz framerate video display on our 0.2” WVGA EVM. A high framerate configuration is excellent for evaluating cutting-edge applications such as augmented reality.

This updated firmware release (v7.3.4) can be installed to any existing DLP LightCrafter Display 2010 Evaluation Module. To do so, the DLP LightCrafter Display GUI software can be used to download the flash image to the board over USB. You can download the latest version of this GUI at: http://www.ti.com/tool/DLPLCRD-GUI. You can find the firmware with 240Hz support at http://www.ti.com/tool/DLPDLCR2010EVM.

If you have any questions about using this firmware, don’t hesitate to reach out to us on the E2E forums.

Best Regards,

Philippe Dollo

If a post answers your question, please click the "Verify Answer" button.

1 Reply

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.