Other Parts Discussed in Thread: DLPC150
Hi,
Let me talk about I2C command between Tiva and DLPC150 on NIRSCAN.
We could not find their command in DLPU031A.
Their command is issued after click Scan button on GUI.
Please let me know their means following.
-0xf1(This is Line 700 in dlpc150.c)
uint8_t cmds[9] = {DLPC150_REG_WRITE, addr, addr>>8, addr>>16, addr>>24, value, value>>8, value>>16, value>>24 };
-0x54(This is Line 534 in dlpc150.c)
uint8_t lampCurrent[7] = {DLPC150_LED_W_CURRENT, 0, 0, 0, 0, 0, 0};
-0x52(This is Line 611 in dlpc150.c)
uint8_t cmds[2] = {DLPC150_LED_W_ENABLE, 0};
-0xda(This is Line 861 in dlpc150.c)
uint8_t cmds[1] = {DLPC150_ADMIN_LIGHT_SENSOR};
-0xf8(This is Line 965 in dlpc150.c)
uint8_t cmds[1] = {DLPC150_SEQ_VECT_NUM};
Best Regards
Hiroyasu