This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPC350: DLPC350 buffer freeze

Part Number: DLPC350
Other Parts Discussed in Thread: DLP4500,

Hi,

I make a new design on the DLPC350 + DLP4500 and the Port 2 (FPD-LINK interface ) has been selected as the video port.

The DMD projection function is ok when i use the internal pattern to test it.

In video mode, the DMD can continue to project hundreds of image stream from FPD-LINK interface .

But i found DLPC350 frame buffer frozen after it receved hundreds of frames. I monitor current read buffer pointer but the value of feed back is not exchange.

I can't find any description about what will lead to the buffer freeze in datasheet or UG.

I have checked the frame timing, it match the spec.

what can I do to troubleshoot the issue?