Hello!
I purchased DLP6500 before.But now it is out of order. The main problems are as follows: Connect to PC, GUI display Unable to switch to video mode. Error: Invalid controller/DMD; State default is standby, click normal and jump back to it; The voltage of EN-OFFSET is zero, and TP20\TP33\TP21 is 3V\0V\0V. The flex cable has slight traces of folding, I wonder if it is damaged.
How should I solve this problem? Thank you.