Hello, I have some questions about offset and hope to get answers.
For structured light measurement and 3D vision applications, can I use 100% offset lightcrafter for point cloud generation?
For calibration and triangle reconstruction algorithms ,is 100% offset device the same as zero offset? Can I use the zero offset algorithm on the 100% offset device? What's the difference between 0 offset and 100% offset devices on point cloud generation algorithms ?Does the 100% offset device's imaging model satisfy pinhole imaging model as the camera?
For 3D vision applications, when using the 100% offset device ,what's the requirement for mounting positions of DLP devices and camera ?What is the difference of mounting positions between zero offset and 100% offset devices?
Thanks & Regards