Hello
I have a question about the difference resolution between x-windows on rasbian and DLPDLCR2000 EVM.
I use DLPDLCR2000 EVM on Raspberry Pi 3 modelB+ and rasbian.
In /boot/config.txt, I set as following:
framebuffer_width=854
framebuffer_hight=480
Then, DLPDLCR2000 EVM can start up X-windows of which the resolution is 854x480.
However, the native resolution of DLPDLCR2000 EVM is 640 x 480.
On X-windows, I start up the windows which has the resolution 840x480, and can display the video in the windows.
Why can the resolution of the video over the native resolution 640x480 be display?
Is the actual resolution of the displayed video 640x480?
Does 854x480 video decrease to 640x480 in actuality?
I would like to get a answer.