Hello,
during the last few weeks, I tried to access a NIRScan nano via C# using HID-USB. This works fine so far: Now it is possible to read temperatures, to set the lamp, to start scans, to read the scan results and so on.
But I have still one last problem to solve: After each scan, I receive e.g. 512 bytes of scan data. How should the scan data received using NNO_CMD_FILE_GET_DATA be interpreted? I know, there is already a method called dlpspec_scan_interpret(). But I can neither find the source code of this method in the example project nor a description of the data model in the EVM User's Guide.
I would be very grateful for a file which describes the structure and the data types of the scan data. A code snippet with the implementation of dlpspec_scan_interpret() would also be very helpful. What I have to know is the meaning and the type of each position in the returned data.
Thanks & Regards,
Simon