This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DLP4710EVM-LC: DLP4710 EVM connects to Basler USB camera external trigger

Intellectual 360 points

Replies: 8

Views: 297

Part Number: DLP4710EVM-LC

Dear Friends

Does any one have experience on Basler USB camera external trigger (from EVM trigger 1 out) coding? Could you please lend me a hand?

I follow the instruction on Basler manual but fail to trigger the camera to grab images (patterns). Below is my setting:

Camera model aca1920-150UC (USB camera)

Camera.TriggerSelector.SetValue( TriggerSelector_FrameStart );
Camera.TriggerMode.SetValue( TriggerMode_On );
Camera.TriggerSource.SetValue ( TriggerSource_Line1 );
Camera.TriggerActivation.SetValue( TriggerActivation_RisingEdge );
Camera.TriggerDelay.SetValue(0);
Camera.ExposureMode.SetValue( ExposureMode_Timed );
Camera.ExposureTime.SetValue( 8000.0 );
Camera.AcquisitionStart.Execute( );

What shall I do next? 

Thank you in advance!

Derlin

 

  • Hello Derlin,


    Are you connecting your camera input to the EVM trigger output? What is the voltage level of the camera? I do not think we have personally used this camera before.

    Thanks,

    Kyle 

  • In reply to Kyle Rakos:

    Hi Kyle,

    I connect EVM trigger 1 (pin4) and ground (pin1) to Basler USB camera GPIO Opto-Isolated input - Line1. The voltage shall be ok because camera accepts 3.3 to 30v.

    I know EVM output can be set to 5V, can't it?

    Thanks!

    Derlin 

     

  • In reply to Derlin Chow:

    Ops, J7 can only set trigger voltage to 3.3 or 1.8V. But I think 3.3v is ok because when I use Basler App (GUI viewer) I can see the camera is grabbing images. Just don't know how to grab the images using c++ code. 

    Another question, if I want to use trigger in to start pattern projection. Shall I use I2C command to set it up? How shall I do it?

    Thanks!

    Derlin

  • In reply to Derlin Chow:

    Hello Kyle/TI

    Is J8 of my EVM is set to accept output trigger or display? I am not sure how you define the pin number.

    If I set the jumper correct, I can send a trigger signal to start the pattern projection?

    Thanks!

    Derlin

      

  • In reply to Derlin Chow:

    Hi Derlin,

    Yes you need to setup the J8 and J9 jumper to setup the trigger in on 3DR pin as mentioned in the user guide page no.10 : http://www.ti.com/lit/ug/dlpu079a/dlpu079a.pdf 

    Thanks,

    Navneet

  • In reply to Navneet Singh:

    Hi Kyle and Navneet,

    I am able to use EVM trigger 2 out to sync with my Basler camera. Thank you! 

    I also want to try trigger in of EVM to project patterns, it seems like the current jumper setting (out of box) is for "trigger in". Am I correct? The board does not mark the pin number.   

    Derlin

  • In reply to Derlin Chow:

    Hi Derlin,

     I am not sure what default configuration comes out of box. You can check at the bottom, pin 1 would be different from pin 2 and pin 3 (pin 1 has the square mark, pin2 and pin3 has circular).

    I hope this helps.

    Thanks,

    Navneet

  • In reply to Navneet Singh:

    Hi Navneet,

    Yes, you  are right, pin1 had square mark. My EVM is set to "trigger in" mode.

    Thank you!

    Derlin

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.