Part Number: DLPD4X00KIT
Hi,
May I ask where to order this type of power connector? It's used to connect the power cord to J12 on the board?
Thanks,
Qiang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DLPD4X00KIT
Hi,
May I ask where to order this type of power connector? It's used to connect the power cord to J12 on the board?
Thanks,
Qiang
Hello Qiang,
These were hand made for the DLPD4X00KIT. The Barrel connector can be 2.1 mm or 2.5 mm ID depending on which Power supply you choose. The OD is 5.5 mm. The other end is specified in the BOM for the particular KIT (see below).
It looks like you have the older style kit pigtail, The newer one is 2 x 2 connectors and the one you show appears to be the 2 x 4 connector.
The 2 x 4 connector on the older controller boards is Molex 43045-0812 which will mate with 43025-0800 receptacle housing. These can be used with female crimp terminals 43030-00nn.
For the 2 x 2 connector on the newer controller boards is Molex 43045-0412 which will mate with 43025-0400 receptacle housing. These also can be used with female crimp terminals 43030-00nn.
The newer board also has a barrel receiving connector that fits 2.5 mm ID and 5.5 mm OD plug - see § 2.2.1 J12 Input Power Connector of DLPU040A - DLP® Discovery™ 4100 Development Platform User's Guide.
This should get you rolling.
Fizix