Other Parts Discussed in Thread: DLP4500
Product: Lightcrafter 4500 (DPLC350)
When using pattern sequence mode, is there a way I can load images to the DLP using USB on the fly instead of those images being displayed through HDMI or "per-stored" images on the flash memory? I was looking at DLPC900 programmers guide and has a feature called "Pattern on-the-fly commands". Is the same possible to be achieved on the DLPC350? If so, how can I achieve this?
Our use for Lightcrafter 4500 is for additive manufacturing. Currently we have to display patterns over HDMI through Raspberry Pi. It would be great if I can load images on the fly directly over USB instead of showing over HDMI. Although I can display per-stored images on the flash memory, it seems this method is not feasible when we have hundreds of patterns we want to load for each experiment. Flashing the ROM takes a very long time.