Hi,
I'd like to purchase this chipset (DLP650LNIR) for my NIR application, but reflectivity data is provided only at @1064 nm. Do you have reflectivity data of the chipset in other wavelength range from 660 nm to 900 nm?
Thanks,
Bryan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'd like to purchase this chipset (DLP650LNIR) for my NIR application, but reflectivity data is provided only at @1064 nm. Do you have reflectivity data of the chipset in other wavelength range from 660 nm to 900 nm?
Thanks,
Bryan
Hello, Bryan. Please see Figure 4 in this application note: http://www.ti.com/lit/an/dlpa031d/dlpa031d.pdf . It shows the transmission curve for the NIR2 window from 350 nm to 2000 nm.
Hi Raecine,
Thanks a lot for the info. Is DLP650LNIR chip covered with NIR2, not NIR?
DMD reflectivity info would be great. Do you have any document that has the data?
Thanks,
Bryan
Yes, the NIR2 curve is the right one for DLP650LNIR. Also, the reflectivity of the micromirrors for the device is listed in the datasheet as nominally 94%. See section 6.10 and 6.11 of the datasheet, http://www.ti.com/lit/ds/symlink/dlp650lnir.pdf.
Thanks!
Yes, I am aware of the nominal reflectivity measured @1064 nm. The NIR region that I am interested in ranges from 660 - 850 nm, and I wonder if the reflectivity would be better or worse than the nominal. Is there any data available?
Sang Hoon Chong
The micro mirror reflectivity matches aluminum, so you can look at the reflectivity curve for aluminum to estimate the micro mirror surface reflectivity versus reflectivity.
Total optical efficiency of the DMD includes window transmission (2 passes) fill factor, diffraction, and micro mirror reflectivity all versus wavelength.
There is an app note on TI.com that covers each of these areas. You can use the math example as a starting point to determine diffraction with your desired wavelength and F numbers.