• TI Thinks Resolved

DLPDLCR2000EVM: Control Individually each Micromirror

Intellectual 1075 points

Replies: 3

Views: 64

Part Number: DLPDLCR2000EVM

Hi Team, we received an inquiry and our customer is asking us if the micromirrors can be controlled individually. We are trying to check the reference but there are no direct answer to confirm the configuration, I am hoping you can help us. Thank you very much

 

DLP LightCrafter Display 2000
DLP® LightCrafter™ Display 2010
DLP® LightCrafter™ Display 3010 G2
DLP LightCrafter Display 3310
DLPC6401-based DLP® Display EVM
DLP® LightCrafter™ Display 4710
DLP® 2010 Light Control Evaluation Module
DLP® NIRscan™ Nano
DLP® 3010 Light Control Evaluation Module

  • Hello Mark,

    Could you please clarify a little bit more what your customer is looking for? All of our DLP chipsets utilize a front end controller which receives video data which is then formatted and sent to the DMD. Some of our light control chipsets are intended to do this with more accurate pixel reproduction - thus essentially achieving individual pixel control.

    Thanks,

    Kyle

  • In reply to Kyle Rakos:

    Hi Kyle,

    Based on the customer's general inquiry they want to use the DMD as light source, a DMD and with a photodiode they want do modulate the light reflected on the DMD according to the flux measured by the photodiode. For than, the optimal solution is to control each micromirror individually and really fast, maybe using a FPGA.

    Thank you for responding.

    Regards,

    Mark

  • In reply to Mark Philip Felipe:

    Hello Mark,

    It sounds like they will want to use one of our light control chipsets such as the DLP2010EVM-LC, DLP3010EVM-LC, or DLP4710EVM-LC. However, it is hard to say without more information. Please feel free to reach out to me offline.

    Thanks,

    Kyle