• TI Thinks Resolved

DLP3010EVM-LC: Compatibility with NVIDIA Jetson family

Intellectual 2265 points

Replies: 1

Views: 28

Part Number: DLP3010EVM-LC

Dear Team,

My customer wanted to confirm if our lightcrafter DLP3010EVM projection technology can work with NVIDIA Jetson family? They wanted to know the compatibility between lightcrafter and NVIDIA Jetson family (nano, TK1/2, xavier). Do we have this test performed?

Your inputs is much appreciated.

Regards,

Renan

  • Hello Renan,

    We do not do testing with specific graphics cards. This EVM has an HDMI input for external video and external patterns. The DLPC3478 controller on the EVM itself accepts parallel video input. In theory, any front end (graphics card, processor, etc.) that complies to HDMI or parallel standards can be used.

    Thanks,

    Kyle