Other Parts Discussed in Thread: DLPC150
Hello,
I had Halogen Lightsource HL-2000 by my side, with a Thorlabs filter at 1550nm and FWHM=12nm. I tried registering spectrum with NIRscan Nano, and I can not get an FWHM at 12nm. I used the parameters used in the document dlpa066.pdf :
Start wavelength— 900 nm
End wavelength— 1700 nm
Pixel width of patterns— 5 px
Number of wavelength points— 427
Number of scans to average— 50
Scan type— column
I measure FWHM=16nm.
I managed to go down to 15nm but no more, with :
Start wavelength— 900 nm
End wavelength— 1700 nm
Pixel width of patterns— 2 px
Number of wavelength points— 623
Number of scans to average— 50
Scan type— column
What would be the parameters to modify to obtain an optimal resolution of 10, as indicated in the user manual?
Thank you, and have a nice day !
Lea