Hello again,
first of all thanks to Eric Pruett who supported me concerning my questions on the use of optical fibers. I decided to use a flexible fiber with 5mm active core diameter. This makes the coupling very easy.
Now I have two more questions:
1. Could You please provide me a 3D model (step file) of NIRScanNano? We would need this to integrate the sensor into an existing machine.
2. The resulting overall measurement time in my project is currently 0.45s. The scan itself takes 0,30s. The process os transfering data via USB takes 0,12s. 0,03s are rquired to do the spectral analysis and to communicate with the PLC. My question: Is it OK that transfering data from the Controller to the PC takes 0,12s? Using USB 2.0 with up to 480 Mbit/s and sending only 3822 Byte of data, I would have estimated a transfer time of less than 1ms. Maybe this is normal, because the controller needs some time for internal calculations!?
Thanks & Regards,
Simon