Other Parts Discussed in Thread: DLPC410, DLPC900
Dear TI forum,
I have a few questions about the DLP® DiscoveryTM 4100 Development Kit .95 1080p (VIS) with DLP9500 1080p chipset:
1) can I control the frame rate of the patterns displayed on the DMD, through software interface (Discovery 4100 Explorer)? Alternatively, in which way can I control this frame rate?
2) what is the maximum pattern rate? Based on the manual I expect it to be 23,148 Hz (1bit), 2,893 Hz (8-bit); can you please confirm?
3) How can I save on the device a set of pre-loaded patterns? When I need to re-use the same set of patterns, I would like to avoid reloading them ... is this possible?
Looking forward to hearing from you.
Best regards
Davide