This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3000-C300REF: DLP3000 cannot boot from NAND, can sometime boot from the SD card, how to fix?

Part Number: DLP3000-C300REF

Dear TI,

I've got one DLP3000 (out of six DLPs on a rig), which gets stuck in the booting sequence.

When I boot from NAND, the DLP stuck at 98% during booting.

When I boot from SD card, sometimes it succeeded, sometimes all the LEDs on the control board (top PCB) are OFF at 98%.

Does that mean the NAND is broken? How can I test/fix it?

Or is there a way to reliably boot from the SD card?

Thanks.

Best,

Joseph Huang