This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DLP3010EVM-LC: How to set all the LED disabled when booting up

Prodigy 190 points

Replies: 2

Views: 26

Part Number: DLP3010EVM-LC

Hi,

I want to set all the LED disabled (=power off) when DLP3010EVM-LC has booted up.

(In other words, I want to set completely dark screen as initial splash screen.)

At the "Update Flash Image" function on the GUI tool, I was able to set black splash screen as default image. But the black splash screen has a bit brightness because LEDs are growing. It's not completely dark screen.

So I tried to creat flash image which set all the LED current to zero as attached png file.

But it's no effect because the minimum of LED current may be 101(mA).

Is it possible to set all the LEDs disabled when DLP3010EVM-LC has booted up ?

  • I'm sorry, I was able to set LED disabled by adding following batch file in the "Update Flash Image" GUI:

  • In reply to user6015626:

    Hello,

    I am glad your were able to resolve the issue.

    Regards,

    Vivek

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.