I am working on an application using DLPC3478 and internal pattern mode. I can successfully project patterns.
However, I am not able to use the API to flip the image. It seems like the projected image is the same, using either of these configurations:
I am wondering if the image flipping is supported using internal pattern mode? And if it is supported, is there any particular order of commands (or similar) that I need to use in order to flip the projected image?