Other Parts Discussed in Thread: DLP4500,
We are currently use this module on a fluorescence microscope, in particular we are using the DLP4500, DLP® 0.45 WXGA DMD for shaping our excitation lasers
We have 4 different lasers on our setup, at 405 488 560 and 640 nm wavelength
I have noticed that the TIR prism that comes with the module is able to overlap the optical path of the 488 and 640 nm, but not the 405 and 488. When the prism is not in place the different wavelengths are reflected at different angles. I guess this comes from the fact that the DLP® LightCrafter™ 4500 module is designed to work with RGB light. Can you confirm this?
My question is: could you provide custom-made prism working at different wavelengths, that on our setup would overlap the reflection of our lasers?