I've followed the below quick start steps but get stuck at the webpage:
- In it, it states to connect the power supply into the power connector, A green LED and a blue LED should light. Done, and LED'S light as stated.
- Next, it instructions me to wait about 10 seconds for the cuvette holder to light up. This happens as stated it would.
- It then tells me that after about 13 seconds the green LED will start flashing, this also starts to flash as expected
- It then states that after about 40 seconds the Blue LED should start to flash also, and once again, this step proceeds as expected.
- I'm then instructed to connect a mini-USB cable from the NIRscan connector labeled "14" to my computer.
I'm told to open a Browser and navigate to http://192.168.0.10 , this is where things start getting flaky. At first I'm returned an "unsecure" message from Chrome Browser, I select to ignore it and attempt to reload, and it will finally connect. I select the option to go to the information screen and from that point on the browser reacts to nothing else.
I disconnect everything and repeat the whole process over, but this time, select another option and once again, from that point on, the interface refuses to accept any more input, I am unable to navigate back to the home page, nothing..
Any ideas on what's going wrong here?
Thanks,
Nick