How to create Visual Studio 2017 project from the source installed from DLP SDK?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to create Visual Studio 2017 project from the source installed from DLP SDK?
Hello David,
Welcome to DLP forum and thank you for your interest in DLP technology.
The SDK project is very old and our team can not provide technical support on this. Please refer to old threads on this subject and follow the past suggestion. Some of the threads for your reference are:
https://e2e.ti.com/support/dlp/f/94/t/778270
https://e2e.ti.com/support/dlp/f/94/t/494611
regards,
Vivek
I succeeded to create VS2017 project and build the DLP_SDK library
I succeeded to create VS2017 project and build the 3D scanning application for Light Crafter 4500
But now, when I run the EXE, I have the following error message:
"The application was unable to start correctly (0xc000007b). Click OK to close the application"
Searching over the web, it looks like mix of 32 & 64 bit code
Any ideas?
Thx in advance and regards
David
The 3D scanning project runs - it should be started in Administrator mode
The 3D scanning application changes patterns and makes frames capture - not as required yet, but from here - it is matter of debugging
The issue can be related to the "debug" configuration of both SDK and 3D Scanning Application
The configuration files are exactly the same (copied) from the EXE file of TI installation - so it should give the same results, and it is not
Any ideas will be wellcomed
Hello David,
I will close this thread since this firmware is not supported by tI.
regards,
Vivek