This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010LC: DLP GUI : "Flash Builder returned with error code 12"

Part Number: DLP3010LC
Other Parts Discussed in Thread: DLP3010EVM-LC

I am using the DLP3010LC GUI, version 2.2.0.6. I am trying to make an updated flash image, that contains some new internal patterns.

I have gone through the steps to create a pattern binary, that I have saved to file.

I have gone through the steps in the "Firmware" section, in order to Update Flash Image. I am using the base firmware input called dlp3010evm-lc_7.3.2.img

As I go through the final step and push "Finish", I get the following error code:

"Flash Builder returned with error code 12"

The GUI does say that "Flash Image Update Completed", but no output is written to file.

I have tried various options searching for something that does not give the error, but I have not been successful.

So my questions:

* What does error code 12 mean?

* How can I avoid it?