The micro USB port from my DLP NIRscan Nano EVM broke of it's solderingpoints, beyond the possibility of resoldering. I contacted the support center, but it is not possible to only replace the driverboard (on which the USB port is located). Is there a way possible way to repair the EVM without buying a new unit? And is it possible to strengten the USB port connection? Because I think it is very fragile for a EVM, especially in this pricerange.