Part Number: DLPLCR6500EVM
I use the DLP® LightCrafter™ 6500 Evaluation Module, to display several patterns (1bitdepth), triggered by an exernal input line.
Communication and control works fine with the GUI provided with the DLP® LightCrafter™ 6500 and 9000 evaluation module. For our application we want to upload our own patterns and start the sequence in the "on the fly pattern mode" in our own software environment (MatLab). Based on the "DLPC900 Programmer's Guide.pdf" document we established communication with the board, and functions like showing internal test patterns works. However uploading and displaying images for "on the fly" mode doesn't work so far, We tried to follow carefully the example 5.3 in the programmers guide. After starting the pattern mode, the displayed pattern is very different from the expected.
We have following questions:
Pattern Display LUT Definition Command: USB(0x1A34): What does Image pattern Index stand for (Byte:11:10)? Isn't this identical to Pattern index (Byte 1:0) ?
Initialize Pattern BMP Load: There are only four Bits for Image Index (Byte which is not eonough to encode dec(511)?
Pattern BMP Load: Do I have to transfer 24Bit patterns, though I need only a grey value with 1bitdepth? Do I have to load pattern with value dec(255) or dec(1) when I want to display in 1 bitdepth?
Looking forward to hearing from you.
Christian