I recently received a Lightcrafter EVM and have been trying to get it to run. I obtained 5V 2400mA power brick for it but when I plug in to the power socket all that happens is a few LEDs turn on: D1 is solid red, D4 is solid green, D2 on the driver board is solid green, and D3 on the driver board flashes red. I have determined that it is going into the shutdown protection mode for the thermistor being above 70 but I don't understand why this is happening. Plus the booting screen has never projected even before the protection shutdown is initiated.
Any help on this issue would be greatly appreciated!
-Kevin