Hi,
I used a 5V with 6A power supply for a DLP3000. It doesn't work anymore. (Right now I know the correct power supply should be 5V with 2-3 A.)
Can I fix it and how?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I used a 5V with 6A power supply for a DLP3000. It doesn't work anymore. (Right now I know the correct power supply should be 5V with 2-3 A.)
Can I fix it and how?
Thank you.
Hi Kaikai,
Using a power supply that is capable of supplying 6A doesn't mean that the Lighcrafter actually draws the full current. It is quite unlikely that you damaged the Lightcrafter with overcurrent.
Can you provide any more details about your lightcrafter - did you have any other symptoms before it broke? Or did you just plug it in one day it doesn't work?
Thanks,
Paul
Hi Paul,
Ah, so 12V is definitely a problem. The device does have some overvoltage protection, but it is possible that you've fried the device.
Use LED D3 (on the bottom board) to help decode your issue:
ON Time | OFF Time | Failure |
1 sec | 10 secs | LED_ENABLE (pin 1 of U11) got triggered because LED_ANODE voltage is greater than 5.8V |
5 sec | 500 msec | SYSPWR Voltage falls to less than 2.7V or greater than 5.2 V |
1.5 secs | 1 sec | Overheat shutdown, GREEN LED thermistor temperature is greater than 70C |
Can you connect your Lightcrafter to the GUI?
-Paul