I am trying to write to an SD card the DM365 NAND.
I get the following error:
C:\Texas Instruments-DLP\DLPLCRSoftwareBundle-3.0\DLP3000-C300REF-DM365-v5.0>lcr_boot_sd.exe lcr_dm365_v5_nand.dat G:
WIN32
Copying image file 'lcr_dm365_v5_nand.dat' to 'G:'
Opening Drive 'G:'
Searching for image file location ..................
Image File Location : 0x1104000
Writing boot record
Error At : lcr_boot_sd.c:435 writeBootRecord!!!
Image copied to SD card SUCCESS
It says SUCCESS but prior there is an error. I am running command prompt as an administrator.
I am trying to do this as my projector gets to 100% on the boot screen and gets stuck.
Thanks