Our LightCrafter got stuck during boot-phase once showing an image of itself in red colors. Problem sounds a bit like first one mentioned in document http://www.ti.com/lit/er/dlpt003/dlpt003.pdf
Since restart no light is emitted anymore, the system doesn't boot and no communication possible.
When switching on the power supply the driver module on the lower side has the green LED next to D3 permanently on, while on the processor boards LED D1 (next to the DM365) (red) and D5 (green) arepermanentely on as well. After around 10s the driver modules red LED (D3) starts flashing in a way indication a thermal shutdown (~1,5/1) and both LEDs on the processor board turn immediately off.
The effect stays the same when unmounting the processor board.
Power supply is a laboratory PS with 5V/5A supplying with about 0.5A during these 10s.
The boards probably have older firmware flashed. There is no "V2" sticker on board or package.
I tried to update the DM365 firmware with an 2GB SD card (no HC) and tried booting from it, which was both unsuccessful.
The LightCrafter is unmodified and was bought in October last year.
I think there is a defect. Anthing else I can do to prove/counter-prove?