Hi,
We are working with the lightcrafter to display a 20 image pattern rapidly (1200 fps). This pattern needs to be synced to a an external motor. We would like to reset the pattern every time the motor makes a full rotation. We are generating the signal for passing the home position ourselves. Is there any way in the API to quickly reset the pattern so that we can sync the two systems reliably? It is important that there is little delay, as the image being projected relies heavily on the location of the motor.