Hi,
We would like to use PWRGOOD signal in order to reset the DLPC900 , is there a minimum time the signal should be LOW in order for the reset to happen?
is there a mechanism to protect against signal spikes ?
Thanks,
Nathan.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We would like to use PWRGOOD signal in order to reset the DLPC900 , is there a minimum time the signal should be LOW in order for the reset to happen?
is there a mechanism to protect against signal spikes ?
Thanks,
Nathan.
Hello Nathan,
Based on the information in the DLPC900 data sheet [ http://www.ti.com/lit/gpn/dlpc900 ] on page 29, this is not a recommended mode of resetting the controller. On the EVM there is no mechanism to protect against "signal" spikes. We assume you mean spikes in the power input. A good DC power supply should filter such spikes out.
I hope this helps.
Fizix
Hi Fizix,
Thanks for the reply, just one more question, how would you recommend doing hardware reset ? the spikes I am talking about are on the signal itself but not due to power supply noise but external noise (EMC ...).
Thanks,
Nathan.
Nathan,
Sorry for the delay. We are still looking at this to determine a recommendation.
Fizix
Hello again Nathan,
I have talked further with the team that designed the EVM. The lead engineer indicates that it is possible to use PWRGOOD provided you send a StandBy command to the system and wait the time prescribed in the controller data sheet before you take PWRGOOD low. You must then also wait the prescribed time after taking PWRGOOD low to allow the micromirrors to finish parking before reasserting PWRGOOD.
This will be equivalent to removing power and the system will go through a full initialization again.
Fizix